LS1088ARDB_2019_0213_1619
=========================
* Version 5

* Errata Fixed:
   [E59]    RST_FORCE2[0] (PORESET) was not implemented though
	    documented.  Added.
   [E60]    LS1088ARDB-PB Rev B adds auto-on support.


LS1088ARDB_2018_1023_1432
=========================
* Version 4

  This image supports:
	LS1088ARDB
      	LS1088ARDB-PB


* Errata Fixed:
    [E58]   Hammering the power button on -PB could lead to entering
	    fault state, requiring AC power cycle.  Still, don't do
	    that.


LS1088ARDB_2018_0912_1356
=========================
* Version 3

  This image supports:
	LS1088ARDB
      	LS1088ARDB-PB


* Errata Fixed:
    [E52]   ALT_HOT_CLK clamped low on -PB.  Unused, as Y11 is
	    typically DNP.
    [E55]   Pushbutton after thermal fault not working correctly
	    for -PB.
    [E56]   Power switch LED not green on stable power for -PB.
    [E57]   PCB_REV reporting incorrect.

* Enhancements:
    [E54]   Import improved power sequencer.


LS1088ARDB_2018_0710_1453
=========================
* Version 2

NOTE: This is a combined image supporting the LS1088ARDB and the new
      LS1088ARDB-PB boards.


* Errata Fixed:
    [E43]   Reset sequencer had incorrect timer implementation; fixed.

* Enhancements:
    [E42]   Watchdog timer support added.  WATCH register added to
	    register file.
    [E44]   Support external power controller for LS1088ARDB-PB.
    [E45]   Report ID=0x4A for LS1088ARDB-PB.
    [E46]   Support enhanced MINTAG data reporting for better alignment
	    with QDS systems.  Drop N.N numbering for simpler N; thus
	    this is now version 2.
    [E47]   Si5341 does not support FINC/FDEC as used, at least officially.
	    Since variable SYSCLK is no longer needed, all this is
	    dropped.
    [E48]   TBSCAN_EN is no longer controlled via CTL.  The switch is
	    still used.  TBSCAN_EN should not be changed post-reset.
    [E50]   STAT0 used for IFC_CS0 (boot from IFC) monitoring.  Since
	    this is now nearly useless, it now monitors I2C1_SCL.
    [E51]   The WARN signal from the SA56004 trips at 70degC vs. 85degC
	    for FAULT.  WARN will drive the LED but now cause a power-down.
	    

NOTE: Though IFC register access is still present, it is deprecated as
      not supported in uboot, and is not validated.  It may be removed
      in future revisions if needed.


LS1088A_RDB_2018_0201
=====================
* Version 1.12

* Errata Fixed:
    [E37]   SDHC_CD and SDHC_WP are on incorrect CPLD pins, register
	    status reads incorrectly.

* Enhancements:
    [E36]   SW team requests software power-off.  PWR_CTL2 (0x21)
	      bit 7 (PWR) now implemented.
    [E38]   EVDD is forced to 1.8V if no card is present, no need for
	      this.  Removed, SW can select either voltage.
    [E39]   VDD_TEMP always asserted causing FAIL usually on.  Mask 
	      with ALARM by default.
    [E40]   Reset timing slow due to SYSCLK change + PLL lock.  These
	      are now skipped if SYSCLK has not been changed in the
	      past.  Reset timing goes from 2.3s to 400ms.
    [E41]   Support Rev D: no ROTATE_ERR, SFP_TX_FAULT/RX_LOS, no QSPI RST.



LS1088A_RDB_2017_0309
=====================
* Version 1.11

* Errata Fixed:
    [E35]   FAIL LED is incorrect polarity, remains on when should
            be off.  Caused by E30 fix, so V1.8 to V1.10 are affected.


LS1088ARDB_2016_1219
====================
* Version 1.10

* Enhancements:
    [E34]   HW devices (NOR, I2CMUX) should be released from reset
            earlier than the DUT.


LS1088ARDB_2016_1010
====================
* Version 1.9

* Enhancements:
    [E33]   LS1088 requires SVDD to power-up before VDD.  Move
            SVDD to tier1.



LS1088ARDB_2016_0824
====================
* Version 1.8

* Errata Fixed:
    [E26]   STAT_PRES2 has bits in wrong order.
    [E27]   RST_CTL[DDRLK] not working.
    [E28]   ROT_ERR not working.  LS1088 does not support this
            feature - DISABLED.
    [E29]   AUTO_ON always occurring.
    [E30]   FAIL LED may be activated when powered off.  LTC
            devices cannot report overtemp when powered off.o

* Enhancements:
    [E31]   Wait ~500ms before powering up after power off in
            AUTO_ON mode.
    [E32]   Enable PRELOAD to dissipate power faster while powering
            off.



LS1088ARDB_2016_0822
====================
* Version 1.7

* Errata Fixed:
    [E24]   TA_BB must default to 1.0V; BRDCFG4 default changed.
    [E25]   RST.RST / RCFG.GO / RESET_REQ did not work because they were
            disabled for testing.  Restored now.

* Enhancements:
    [E20]   Add address mux rotation to support LS1046 as well as LS1043
            [CPU_ID based].
    [E21]   Connect RST_FORCE2[6]/RST_MASK2[6] to SI5341, principally to
            allow SW to reprogram SerDes clocks.  Experimental use only.
    [E22]   Alter BRDCFG5[3:2] definition as follows:
                0X  = AUTO SD/EMMC Mode.
                        If card installed, connect SPI/SDHC to SD slot.
                        Else connect to eMMC.
                10  = FORCE SDHC Mode.
                        SPI/SDHC pins connect to SD slot always.
                11  = FORCE EMMC Mode.
                        SPI/SDHC pins connect to eMMC device always.
            RM will be updated shortly.
    [E23]   Allow concurrent access to registers from I2C or IFC.  SW4#7
            is now unused.

* Passes regression tests.



LS1088ARDB_2016_0525
====================
* Version 1.6

* Errata Fixed:
    [E14]   Use HOT_CLK (H12) to allow XOSC to be DNP.
    [E15]   IFC_CLK is on pin J12 (unused)
    [E18]   cfg_rstreq_md is now 1 bit.
    [E19]   RST_REASON corrected.

* Enhancements:
    [E16]   Add QMAP values to allow QSPI devices to be programmed externally.
            NOTE: The DediProg EM100 does not support this.

    [E17]   Convert RST_QSPI_B to an input to allow QSPI emulators to trigger
            reset.
            NOTE: The DediProg EM100 does not support this.



LS1088ARDB_2016_0308
====================
* Version 1.5

* Errata Fixed:
    [E12]   Bypass clock delay to speed boot if not changing SYSCLK.

    [E13]   Change RUN LED to ASLEEP for cross-system compatibility. 


LS1088ARDB_2016_0113
====================
* Version 1.1

* Errata Fixed:
    [E1..E11]   See tracker.


LS1088ARDB_2015_0831_0954
=========================
* Version 1
* Prototype build - untested